Enabling CoreSight on i.MX 8MM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling CoreSight on i.MX 8MM

Jump to solution
9,402 Views
kanimozhi_t
Contributor V

Hi,

 

    We're using Yocto Zeus and would like to embed CoreSight for hardware assisted tracing. We enable this by integrating opencsd to the perf tool, but the source and sink drivers are missing.

    We verified that the kernel is configured correctly to include the CoreSight modules but the device tree is lacking the hw trace addresses for etm.

    So we request you to provide the etm address for the A53 cores and the related data. It would be helpful if you could share the example Device tree with coresight enabled.

    Another question is that how can we include coresight into the perf tool? As the included perf recipe is missing the coresight package configuration.

 

Thanks in advance.

Labels (2)
0 Kudos
Reply
1 Solution
9,248 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You should change like:

status = "okay";

View solution in original post

8 Replies
9,364 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Since 8MM shares same cores' design as 8MP, you can take reference of how to define ETM and related coresight nodes on 8MP: arch/arm64/boot/dts/freescale/imx8mp.dtsi. The coresight driver in kernel is create PMU events for perf, so after you enabled coresight driver, perf can see it: https://www.kernel.org/doc/Documentation/trace/coresight.txt

0 Kudos
Reply
9,356 Views
kanimozhi_t
Contributor V

Thanks @Zhiming_Liu for your valuable information.

I've added the following lines from im8mp.dtsi (with modified clocks, IMX8MP_CLK_MAIN_AXI -> IMX8MQ_CLK_MAIN_AXI)

etm0: etm@28440000 {
    compatible = "arm,coresight-etm4x", "arm,primecell";
    reg = <0x0 0x28440000 0x0 0x10000>;
    arm,primecell-periphid = <0xbb95d>;
    cpu = <&A53_0>;
    clocks = <&clk IMX8MQ_CLK_MAIN_AXI>;
    clock-names = "apb_pclk";
    status = "disabled";

        out-ports {
            port {
            etm0_out_port: endpoint {
                remote-endpoint = <&ca_funnel_in_port0>;
            };
        };
    };
};

etm1: etm@28540000 {
    compatible = "arm,coresight-etm4x", "arm,primecell";
    reg = <0x0 0x28540000 0x0 0x10000>;
    arm,primecell-periphid = <0xbb95d>;
    cpu = <&A53_1>;
    clocks = <&clk IMX8MQ_CLK_MAIN_AXI>;
    clock-names = "apb_pclk";
    status = "disabled";

    out-ports {
        port {
            etm1_out_port: endpoint {
                remote-endpoint = <&ca_funnel_in_port1>;
            };
        };
    };
};

etm2: etm@28640000 {
    compatible = "arm,coresight-etm4x", "arm,primecell";
    reg = <0x0 0x28640000 0x0 0x10000>;
    arm,primecell-periphid = <0xbb95d>;
    cpu = <&A53_2>;
    clocks = <&clk IMX8MQ_CLK_MAIN_AXI>;
    clock-names = "apb_pclk";
    status = "disabled";

    out-ports {
        port {
            etm2_out_port: endpoint {
                remote-endpoint = <&ca_funnel_in_port2>;
            };
        };
    };
};

etm3: etm@28740000 {
    compatible = "arm,coresight-etm4x", "arm,primecell";
    reg = <0x0 0x28740000 0x0 0x10000>;
    arm,primecell-periphid = <0xbb95d>;
    cpu = <&A53_3>;
    clocks = <&clk IMX8MQ_CLK_MAIN_AXI>;
    clock-names = "apb_pclk";
    status = "disabled";

    out-ports {
        port {
            etm3_out_port: endpoint {
                remote-endpoint = <&ca_funnel_in_port3>;
            };
        };
    };
};

funnel0: funnel {
        /*
    * non-configurable funnel don't show up on the AMBA
    * bus.  As such no need to add "arm,primecell".
    */
    compatible = "arm,coresight-static-funnel";
    status = "disabled";

    in-ports {
        #address-cells = <1>;
        #size-cells = <0>;

        port@0 {
            reg = <0>;
            ca_funnel_in_port0: endpoint {
                remote-endpoint = <&etm0_out_port>;
            };
        };

        port@1 {
            reg = <1>;
            ca_funnel_in_port1: endpoint {
                remote-endpoint = <&etm1_out_port>;
            };
        };

        port@2 {
            reg = <2>;
            ca_funnel_in_port2: endpoint {
                remote-endpoint = <&etm2_out_port>;
            };
        };

        port@3 {
            reg = <3>;
            ca_funnel_in_port3: endpoint {
                remote-endpoint = <&etm3_out_port>;
            };
        };
    };

    out-ports {
        port {
            ca_funnel_out_port0: endpoint {
                remote-endpoint = <&hugo_funnel_in_port0>;
            };
        };
    };

};

funnel1: funnel@28c03000 {
    compatible = "arm,coresight-dynamic-funnel", "arm,primecell";
    reg = <0x0 0x28c03000 0x0 0x1000>;
    clocks = <&clk IMX8MQ_CLK_MAIN_AXI>;
    clock-names = "apb_pclk";
    status = "disabled";

    in-ports {
        #address-cells = <1>;
        #size-cells = <0>;

        port@0 {
            reg = <0>;
            hugo_funnel_in_port0: endpoint {
                remote-endpoint = <&ca_funnel_out_port0>;
            };
        };

        port@1 {
            reg = <1>;
            hugo_funnel_in_port1: endpoint {
                /* M7 input */
            };
        };

        port@2 {
            reg = <2>;
            hugo_funnel_in_port2: endpoint {
                /* DSP input */
            };
        };
        /* the other input ports are not connect to anything */
    };

    out-ports {
        port {
            hugo_funnel_out_port0: endpoint {
                remote-endpoint = <&etf_in_port>;
            };
        };
    };
};

etf@28c04000 {
    compatible = "arm,coresight-tmc", "arm,primecell";
    reg = <0x0 0x28c04000 0x0 0x1000>;
    clocks = <&clk IMX8MQ_CLK_MAIN_AXI>;
    clock-names = "apb_pclk";
    status = "disabled";

    in-ports {
        port {
            etf_in_port: endpoint {
                remote-endpoint = <&hugo_funnel_out_port0>;
            };
        };
    };

    out-ports {
        port {
            etf_out_port: endpoint {
                remote-endpoint = <&etr_in_port>;
            };
        };
    };
};

etr@28c06000 {
    compatible = "arm,coresight-tmc", "arm,primecell";
    reg = <0x0 0x28c06000 0x0 0x1000>;
    clocks = <&clk IMX8MQ_CLK_MAIN_AXI>;
    clock-names = "apb_pclk";
    status = "disabled";

    in-ports {
        port {
            etr_in_port: endpoint {
                remote-endpoint = <&etf_out_port>;
            };
        };
    };
};
 
However, the /sys/bus/coresight/devices/ are still empty:
root@imx8mq:/# ls -la /sys/bus/coresight/devices/
total 0
drwxr-xr-x 2 root root 0 Jan 13 10:46 .
drwxr-xr-x 4 root root 0 Jan 13 10:46 .. 
 
But I got the ETM Modules, listed as follows
root@imx8mq:/# find . -name "*etm*"
./usr/bin/setmetamode
./sys/devices/cs_etm
./sys/bus/amba/drivers/coresight-etm4x
./sys/bus/event_source/devices/cs_etm
./sys/firmware/devicetree/base/etm@28740000
./sys/firmware/devicetree/base/etm@28640000
./sys/firmware/devicetree/base/etm@28540000
./sys/firmware/devicetree/base/etm@28440000
./sys/module/coresight_etm4x

 

So, my questions are:

1. How to make available of the CoreSight sinks and sources?

 

2. How to check the perf tool for CoreSight integration?

 

Thanks in advance!
0 Kudos
Reply
9,294 Views
kanimozhi_t
Contributor V

To add additional context, I've taken the lines related to CoreSight (EMT, Funnel, etc.,) lines from the "imx8mp.dtsi" file and paste the same in the "imx8mq.dtsi" file.

During this process, I had to change the "IMX8MP_CLK_MAIN_AXI" to "IMX8MQ_CLK_MAIN_AXI" for mitigating the build errors. Apart from this change the build succeeds without any further modifications.

But even after this addition in device tree, the Linux filesystem does not include any of the CoreSight devices.

So, it raises the following questions:

  1. Is the address of ETM for i.MX 8MP and i.MX 8MQ same? Eg: for etm1
    reg = <0x0 0x28440000 0x0 0x10000>;
  2. What is the purpose of the line status = "disabled" ? Do I need to enable it?
  3. Where can I find the ETM addresses for i.MX 8MQ?
0 Kudos
Reply
9,273 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

1.The ETM address of i.MX8M series is same.They are the same cpu ip.

2.You must enable it if you wants to use node

BR

Zhiming

9,257 Views
kanimozhi_t
Contributor V

Even after enabling all the nodes in the above Device Tree fragment above as,

status = "enabled";

the CoreSight devices are empty in the Linux.

Do you have any idea of what would've gone wrong or further debugging steps?

Tags (2)
0 Kudos
Reply
9,249 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You should change like:

status = "okay";
9,232 Views
kanimozhi_t
Contributor V

@Zhiming_Liu Thanks for your swift replies and helping us to get it worked.

0 Kudos
Reply
9,380 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

I have asked the expert and will update later

0 Kudos
Reply