Enable clk02 output on mx8mq

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Enable clk02 output on mx8mq

跳至解决方案
1,048 次查看
vanpye00
Contributor II

Hi,

I'm trying to make the imx8mq to output the 24mhz clock signal on its own per this post https://community.nxp.com/t5/i-MX-Processors/enable-CLKO2-for-24MHz-output-clock-on-iMX8MN/m-p/12776... but it's not outputing anything. Is there anything difference should I do for the imx8mq?

0 项奖励
回复
1 解答
995 次查看
vanpye00
Contributor II

I got it to work now.

I'm current using kernel Hardknott. It turns out, for Hardknott, uboot was auto-selecting the customboard legacy dts rather than the customboard dts, which was what I modified. Reconfigured uboot to select the customboard dts resolved the issue.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,030 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You must check if your GPIO pads are the same ad the MX8MNano, if not change it and should be working.

regards

0 项奖励
回复
996 次查看
vanpye00
Contributor II

I got it to work now.

I'm current using kernel Hardknott. It turns out, for Hardknott, uboot was auto-selecting the customboard legacy dts rather than the customboard dts, which was what I modified. Reconfigured uboot to select the customboard dts resolved the issue.

0 项奖励
回复