Enable Spread Spectrum on IMX8M-Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable Spread Spectrum on IMX8M-Mini

3,056 Views
mayqueen
Contributor IV

As title, I just find the IMX8QX-Plus has official Spread Spectrum instruction as following:

User Guide of Spread Spectrum Support for i.MX 8QuadMax and i.MX 8QuadXPlus Display 

But there are many difference between IMX8QX-PLUS and IMX8M-Mini, I need IMX8M-Mini relate instruction, does the NXP official can provide it? Thanks a lot

May

Labels (1)
0 Kudos
Reply
3 Replies

2,923 Views
igorpadykov
NXP Employee
NXP Employee

Hi May

unfortunately I am not aware of similar documentation for i.MX8M Mini, but

it is supported and described in sect.5.1.5.4.4 SSCG and Fractional PLLs  i.MX8M Mini  RM

i.MX 8M Mini Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,923 Views
mayqueen
Contributor IV

So how to implement spread spectrum on IMX8M-Mini, I have no idea after I saw that section of RM file as you send, do you have example codes?

Thanks

0 Kudos
Reply

2,923 Views
igorpadykov
NXP Employee
NXP Employee

Hi May

 

unfortunately I am not aware of example codes. So you will have to

develop them himself or apply for help to Commercial Support and Engineering Services | NXP 

to develop them.

Best regards
igor

0 Kudos
Reply