Enable Multi Display in iMX8QM running Android Automotive OS 11.0.0_2.3.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enable Multi Display in iMX8QM running Android Automotive OS 11.0.0_2.3.0

2,272 次查看
swapnil
Contributor I

Hello,

I am trying to enable multi display function in Android Automotive OS 11.0.0_2.3.0 running on iMX8QM. We want to enable HDMI_TX as the default display interface for the Android Automotive OS primary display rather than LVDS.


I have referred the Android User's Guide and have performed the steps mentioned in the document.
The steps are:

  1. Into the uboot mode, entered the fastboot mode using fastboot 0.
  2. Then, flashed the dtbo-imx8qm-md.img & vbmeta-imx8qm-md.img to their respective partitions.


Further, I am unable to see anything on the display connected through the HDMI_TX port.

Would appreciate the response to resolve this.

 

Thanks!!

0 项奖励
回复
5 回复数

2,204 次查看
swapnil
Contributor I

But the documentation suggest that Android Automotive OS 11 also support multi display functionality. However, with the above steps, the android system is not detecting the HDMI display.

0 项奖励
回复

2,200 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

You may try android automotive 13 or 14, where the hdmi is working.

regards

0 项奖励
回复

2,195 次查看
swapnil
Contributor I

Hello,

I have tried with Android Automotive OS 14 also on NXP i.MX8QM. The results are still same - "unable to see anything on the display connected through HDMI". The android system doesn't detect the HDMI display. 

0 项奖励
回复

2,156 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

Just tried to boot the MX8QM with Android and everything works ok on hdmi, maybe is a problem with the hardware of HDMI, I can see the HDMI-TX with J6.

Regards

0 项奖励
回复

2,235 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

For android 11 does not include support for dual display, you may try android 13 or 14 however if you want to try, try this:

Please refer to it.

&mipi0_disp {
    compatible = "fsl,imx8mp-mipi-display";
    disp-type = "mipi-dsi";
    status = "okay";
    port@0 {
        endpoint {
            remote-endpoint = <&dpu1_mipi0>;
        };
    };
};

&lvds0_disp {
    compatible = "fsl,imx8mp-lvds-display";
    disp-type = "lvds";
    status = "okay";
    port@0 {
        endpoint {
            remote-endpoint = <&dpu1_lvds0>;
        };
    };
};

For more details please refer to the location given below.
Documentation/devicetree/bindings/display/

 

Regards

0 项奖励
回复