Enable IMX8QXP LSIO PWM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable IMX8QXP LSIO PWM

ソリューションへジャンプ
4,451件の閲覧回数
paul_katarzis
Contributor III

I am working with a custom board that requires UART1_RTS_B to be used as a PWM output. I have currently configured our device tree to set the mux_mode of UART1_RTS_B to LSIO_PWM2_OUT. Our device tree is based on the following DTSI files from NXP: fsl-imx8qxp.dtsi, fsl-imx8dxp.dtsi, fsl-imx8dx.dtsi, and fsl-imx8-ca35.dtsi. I did not see any nodes in these files for the LSIO PWM modules and I did not see them enabled in the device tree for the IMX8QXP MEK. Therefore I have to write my own node for LSIO PWM 2. What I have written so far is based on the pwm_adma_lcdif, pwm_mipi_lvds0, and pwm_mipi_lvds1 nodes in fsl-imx8dx.dtsi:

pwm2: pwm@5d020000 {
compatible = "fsl,imx8qxp-pwm", "fsl,imx27-pwm";
reg = <0x0 0x5d020000 0x0 0x10000>;
clocks = <&clk IMX8QXP_LSIO_PWM2_IPG_S_CLK>,
<&clk IMX8QXP_LSIO_PWM2_CLK>;
clock-names = "ipg", "per";
assigned-clocks = <&clk IMX8QXP_LSIO_PWM2_CLK>;
assigned-clock-rates = <24000000>;
#pwm-cells = <2>;
power-domains = <&pd_lsio_pwm2>;
status = "okay";
};

I noticed that nodes such as pwm_adma_lcdif have the size cells of the reg property set to 0x0 0x1000, even though the memory map shows that region is 64KB. Should I also set the size cells of the reg property of my PWM node to 0x0 0x1000 even though the memory map says it is 64KB?

I found that dt-bindings/clock/imx8qxp-clock.h has the following clocks defined for LSIO PWM 2: IMX8QXP_LSIO_PWM2_DIV, IMX8QXP_LSIO_PWM2_IPG_S_CLK, IMX8QXP_LSIO_PWM2_IPG_SLV_CLK, IMX8QXP_LSIO_PWM2_IPG_MSTR_CLK, IMX8QXP_LSIO_PWM2_HF_CLK, and IMX8QXP_LSIO_PWM2_CLK. I could not find an explanation for what these clocks do. What is the difference between the IPG_S, IPG_SLV, and IPG_MSTR clocks and which should be used for the IPG clock in my PWM node? Should the PER clock be set with the IMX8QXP_LSIO_PWM2_CLK or some other clock? Are the assigned-clocks and assigned-clock-rates properties set correctly in my PWM node?

ラベル(1)
1 解決策
4,128件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Paul

one can look at example from i.MX8QXP-B0 L4.9.88_2.2.0-8qxp_beta2 release

for LSIO_PWM0 (use pin SC_P_UART1_TX_LSIO_PWM0_OUT) and try to port it.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
4,129件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Paul

one can look at example from i.MX8QXP-B0 L4.9.88_2.2.0-8qxp_beta2 release

for LSIO_PWM0 (use pin SC_P_UART1_TX_LSIO_PWM0_OUT) and try to port it.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,128件の閲覧回数
paul_katarzis
Contributor III

This is very helpful. Thank you, Igor!

0 件の賞賛
返信