Enable I.MX 6 USB 3.0 Feature

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enable I.MX 6 USB 3.0 Feature

3,472 次查看
brightwang
Contributor III

Is Anyone There Can Help To This Problem With USB 3.0? We Have A Working Project Bases On I.MX6Q Application Processor But Unfortunately I.MX6Q Has No USB 3.0 Support. So We Find This TUSB9261 TI's USB 3.0 To SATA Bridge. Is That Possible Use The Bridge M3 IC To Enable USB 3.0 Features?

TUSB9261 | USB Peripheral | USB | Description & parametrics 

标签 (1)
标记 (4)
0 项奖励
回复
3 回复数

2,704 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   I am afraid TUSB9261  is just USB to SATA bridge.

It does not add USB3 functionality to i.MX6 in itself.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,704 次查看
brightwang
Contributor III

So Is It No Way To Enable USB 3.0 Features Upon I.MX6Q? I Find Some PCIe Gen2 To xHCI But They Are Not Qualified With AEC-Q100.

0 项奖励
回复

2,704 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The best way to get USB3 with i.MX6 - using a PCIe-to-USB3 converter. 

Regards,

Yuri.

0 项奖励
回复