Enable I.MX 6 USB 3.0 Feature

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable I.MX 6 USB 3.0 Feature

1,934件の閲覧回数
brightwang
Contributor III

Is Anyone There Can Help To This Problem With USB 3.0? We Have A Working Project Bases On I.MX6Q Application Processor But Unfortunately I.MX6Q Has No USB 3.0 Support. So We Find This TUSB9261 TI's USB 3.0 To SATA Bridge. Is That Possible Use The Bridge M3 IC To Enable USB 3.0 Features?

TUSB9261 | USB Peripheral | USB | Description & parametrics 

ラベル(1)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

1,166件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   I am afraid TUSB9261  is just USB to SATA bridge.

It does not add USB3 functionality to i.MX6 in itself.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,166件の閲覧回数
brightwang
Contributor III

So Is It No Way To Enable USB 3.0 Features Upon I.MX6Q? I Find Some PCIe Gen2 To xHCI But They Are Not Qualified With AEC-Q100.

0 件の賞賛
返信

1,166件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The best way to get USB3 with i.MX6 - using a PCIe-to-USB3 converter. 

Regards,

Yuri.

0 件の賞賛
返信