En/Decryption of data on iMX6 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

En/Decryption of data on iMX6 board

ソリューションへジャンプ
11,315件の閲覧回数
rashmi
Contributor III

Hi,

How do I set up a CAAM  to en/decrypt a data on a iMX6 SABRE board? Are there any sample application available?

I have gone through Security Reference manual which gives me low level information, does not seem of too much help to me.

Thanks

1 解決策
7,870件の閲覧回数
Yuri
NXP Employee
NXP Employee

The Platform SDK (after cross-compiling) provides executable images (.elf, .bin), that should be run on a target board (say, on i.MX6 SDP).

Please to run .elf on the SDP, using a JTAG debugger.

元の投稿で解決策を見る

0 件の賞賛
返信
23 返答(返信)
646件の閲覧回数
LaurenPost
NXP Employee
NXP Employee

We just released 3.10.9-1.0.0 alpha a BSP release under Yocto back in October.  Next we are planning a 3.10.17-1.0.0_beta release for Yocto in early 2014.  This is a Linux BSP release.  We no longer release ltib releases for Linux.

0 件の賞賛
返信
646件の閲覧回数
XXiao1z
Contributor III

I'm using repo with fsl-community-bsp-platform, how can I find the specific BSP release(e.g. 3.10.9-1.0.0 alpha BSP)? or am I missing something? all I saw is 1.4 release, 1.5 release at github and I did not find any tag for the BSP you mentioned. do you mean just the kernel release? I'm confused.

Thanks,

0 件の賞賛
返信
646件の閲覧回数
rashmi
Contributor III

So Can I use openssl commands with cryptodev engine to encrypt and decrypt data files?

Can you please brief me on how does cryptodev through openssl can access the CAAM support.

Are there any user space C application.

Thanks

0 件の賞賛
返信