Edit OS settings before buiding desktop image using yocto on imx8mplus-evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Edit OS settings before buiding desktop image using yocto on imx8mplus-evk

1,955件の閲覧回数
sanum19
Contributor III

I need to change the default display setting of sleep to "Never" before the image is being build. Im trying this on latest yocto desktop image to be run on imx8mplus-evk.

Please give me guidance to how to achieve this.

0 件の賞賛
返信
3 返答(返信)

1,941件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

I think you can base here, download the layer that has that config and modify it, it shouldn't be re-downloaded and keep your configuration, which you should look for.

Regards

0 件の賞賛
返信

1,898件の閲覧回数
sanum19
Contributor III

i couldnt find the layer that has that config.

Since i'm trying to build desktop image . Usually in ubuntu these configurations can be controlled by editing /etc/systemd/logind.conf .Can i do the same edits in yocto sdk , so that it will get reflected in bitbaked image?

スポイラ
 
0 件の賞賛
返信

1,882件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Desktop calls BSP code plus:

<?xml version="1.0" encoding="UTF-8"?>
<manifest>

  <include name="imx-6.1.55-2.2.0.xml"/>

  <project name="meta-nxp-desktop" remote="nxp-imx" path="sources/meta-nxp-desktop" revision="refs/tags/rel_lf_6.1.55_2.2.0_ldp" upstream="lf-6.1.55-2.2.0-mickledore" >
    <linkfile src="tools/imx-setup-desktop.sh" dest="imx-setup-desktop.sh"/>
    <linkfile src="README.md" dest="README-DESKTOP"/>
  </project>

</manifest>

Here is the layer repo.

There are not overrides in our Proof of Concept, but you could rework this with a custom layer on top of this looking to override the specific file (logind.conf), I found this post that gathers different approaches to overriding a RFS file.

Regards

0 件の賞賛
返信