[ERROR] : SWUPDATE failed [0] ERROR : Error: Cannot read default environment from file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[ERROR] : SWUPDATE failed [0] ERROR : Error: Cannot read default environment from file

跳至解决方案
4,348 次查看
wang12zhe
Contributor III

HW: IMX8QXP

BSP: L5.10.52

I want to update firmware by swupdate, so I add swupdate to Yocto and download to board and add fw_printenv/fw_setenv to system and work well. Then

root@imx8qxpmek:~# swupdate -w "--document-root /www --port 8999"
Swupdate v2021.11.0

Licensed under GPLv2. See source distribution for detailed copyright notices.

Connected to SWUpdate via /tmp/swupdateprog

At this moment I can open the web on PC and try to update a signal file but always show:

[INFO ] : SWUPDATE started : Software Update started !
[ERROR] : SWUPDATE failed [0] ERROR : Error: Cannot read default environment from file
[INFO ] : SWUPDATE running : Installation in progress
[ERROR] : SWUPDATE failed [0] ERROR : Error: Cannot read default environment from file
[ERROR] : SWUPDATE failed [0] ERROR : Error: Cannot read default environment from file
[ERROR] : SWUPDATE failed [0] ERROR : Cannot persistently store INSTALLED update state.
[ERROR] : SWUPDATE failed [1] Installation failed !
[INFO ] : No SWUPDATE running : Waiting for requests...

 

Why always show this error and how to fix it ?

 

 

 

 

 

 

 

 

0 项奖励
回复
1 解答
4,302 次查看
wang12zhe
Contributor III

Yes, my fw_printenv working well.

But when I do "saveenv" in uboot,this error will be fixed

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,322 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @wang12zhe,

I hope you are doing well.

Please make sure that /etc/fw_env.config is present and has the correct information about the environment device, offset & size.

Thanks & Regards,
Dhruvit Vasavada

0 项奖励
回复
4,303 次查看
wang12zhe
Contributor III

Yes, my fw_printenv working well.

But when I do "saveenv" in uboot,this error will be fixed

0 项奖励
回复