ERROR: Nothing PROVIDES 'core-image-minimal'

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ERROR: Nothing PROVIDES 'core-image-minimal'

13,589件の閲覧回数
victorgomez
Contributor II

Hi All,

I am trying to build my Yocto 2.0 jethro kernel and when I type "bitbake <image>", it always tells me the same error:

ERROR: Nothing PROVIDES 'core-image-minimal'

It doesn't matter which image name I pass. It is always the same error.

Does anybody know what I am doing wrong?

Thanks a lot in advance!

ラベル(1)
3 返答(返信)

8,339件の閲覧回数
lily95
Contributor I

I have almost the same problem, the problem is ERROR: Nothing PROVIDES 's32g274ardb' ,and my local.conf below:

MACHINE ??= 's32g274ardb'
DISTRO ?= 'fsl-auto'
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES ?= "debug-tweaks"
USER_CLASSES ?= "buildstats image-mklibs image-prelink"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS ??= "\
STOPTASKS,${TMPDIR},1G,100K \
STOPTASKS,${DL_DIR},1G,100K \
STOPTASKS,${SSTATE_DIR},1G,100K \
STOPTASKS,/tmp,100M,100K \
ABORT,${TMPDIR},100M,1K \
ABORT,${DL_DIR},100M,1K \
ABORT,${SSTATE_DIR},100M,1K \
ABORT,/tmp,10M,1K"
PACKAGECONFIG_append_pn-qemu-system-native = " sdl"
CONF_VERSION = "1"

# Parallelism Options
BB_NUMBER_THREADS = "112"
PARALLEL_MAKE = "-j 84"
DL_DIR = "/usr1/bsp1115/fsl-auto-yocto-bsp/downloads"
SSTATE_DIR = "/usr1/bsp1115/fsl-auto-yocto-bsp/sstate-cache"
INHERIT += "own-mirrors"
SOURCE_MIRROR_URL ?= "http://git.freescale.com/source/"
SSTATE_MIRRORS = "file://.*/(.*)/(.*) file://${SSTATE_DIR}/native/\1/\2 \n"
# use xz to compress sstate
SSTATE_PKG_SUFFIX = "txz"
SSTATE_PKG_TARZIPPROG = "xz"
ACCEPT_FSL_EULA = "1"

any suggestion will be helpfull~

THANKS!

0 件の賞賛
返信

9,341件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Victor Gomez,

Could you share your conf/local.conf file settings? It is possible that the machine and distro configuration is not correct and thus is not finding the recipes for the image. Did the repo sync finished successfully? Another possibility is that the metadata was not downloaded correctly.

Regards,

9,340件の閲覧回数
victorgomez
Contributor II

Hi :smileyhappy:

The repo sync finished successfully, yes. This is the content of local.conf:

MACHINE ??= 'imx7dsabresd'

DISTRO ?= 'poky'

PACKAGE_CLASSES ?= "package_rpm"

EXTRA_IMAGE_FEATURES = "debug-tweaks dbg-pkgs dev-pkgs package-management ssh-server-dropbear ssh-server-openssh staticdev-pkgs tools-debug tools-sdk x11 x11-base ypbind-mt"

USER_CLASSES ?= "buildstats image-mklibs"

PATCHRESOLVE = "noop"

BB_DISKMON_DIRS = "\

    STOPTASKS,${TMPDIR},1G,100K \

    STOPTASKS,${DL_DIR},1G,100K \

    STOPTASKS,${SSTATE_DIR},1G,100K \

    STOPTASKS,/tmp,100M,100K \

    ABORT,${TMPDIR},100M,1K \

    ABORT,${DL_DIR},100M,1K \

    ABORT,${SSTATE_DIR},100M,1K \

    ABORT,/tmp,10M,1K"

PACKAGECONFIG_append_pn-qemu-native = " sdl"

PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"

CONF_VERSION = "1"

DL_DIR ?= "${BSPDIR}/downloads/"

ACCEPT_FSL_EULA = "1"

0 件の賞賛
返信