ERROR : HID(R):LIBUSB_ERROR_TIMEOUT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ERROR : HID(R):LIBUSB_ERROR_TIMEOUT

Jump to solution
6,143 Views
embedded_Dev
Contributor III

Hi ,

We are using a customized board based on IMX6UL evk NXP board. We are using the RAM D2516ECMDXGME-U

I have tested the callibration and stress tests. I filled the values from the callibration test in imximage.cfg.

I compiled the u-boot and i filled the values in board/freescale/mx6ul_14x14_evk/imximage.cfg

The following are the values from the files imximage.cfg

----------------------------------------------------------------------------------------

/*
* Copyright (C) 2015 Freescale Semiconductor, Inc.
* Copyright 2017 NXP
*
* SPDX-License-Identifier: GPL-2.0+
*
* Refer docs/README.imxmage for more details about how-to configure
* and create imximage boot image
*
* The syntax is taken as close as possible with the kwbimage
*/

#define __ASSEMBLY__
#include <config.h>

/* image version */

IMAGE_VERSION 2

/*
* Boot Device : one of
* spi/sd/nand/onenand, qspi/nor
*/

#ifdef CONFIG_QSPI_BOOT
BOOT_FROM qspi
#elif defined(CONFIG_NOR_BOOT)
BOOT_FROM nor
#else
BOOT_FROM sd
#endif

#ifdef CONFIG_USE_IMXIMG_PLUGIN
/*PLUGIN plugin-binary-file IRAM_FREE_START_ADDR*/
PLUGIN board/freescale/mx6ul_14x14_evk/plugin.bin 0x00907000
#else

#ifdef CONFIG_IMX_HAB
CSF CONFIG_CSF_SIZE
#endif

/*
* Device Configuration Data (DCD)
*
* Each entry must have the format:
* Addr-type Address Value
*
* where:
* Addr-type register length (1,2 or 4 bytes)
* Address absolute address of the register
* value value to be stored in the register
*/


/* DDR type MT41K256M16HA-125 which is EOL */

/* Enable all clocks */
DATA 4 0x020c4068 0xffffffff
DATA 4 0x020c406c 0xffffffff
DATA 4 0x020c4070 0xffffffff
DATA 4 0x020c4074 0xffffffff
DATA 4 0x020c4078 0xffffffff
DATA 4 0x020c407c 0xffffffff
DATA 4 0x020c4080 0xffffffff

DATA 4 0x020D8004 0x00000872
DATA 4 0x020D801C 0x01000041

#ifdef CONFIG_IMX_OPTEE
DATA 4 0x20e4024 0x00000001
CHECK_BITS_SET 4 0x20e4024 0x1
#endif

DATA 4 0x020E04B4 0x000C0000
DATA 4 0x020E04AC 0x00000000
DATA 4 0x020E027C 0x00000030
DATA 4 0x020E0250 0x00000030
DATA 4 0x020E024C 0x00000030
DATA 4 0x020E0490 0x00000030
DATA 4 0x020E0288 0x00000030
DATA 4 0x020E0270 0x00000000
DATA 4 0x020E0260 0x00000030
DATA 4 0x020E0264 0x00000030
DATA 4 0x020E04A0 0x00000030
DATA 4 0x020E0494 0x00020000
DATA 4 0x020E0280 0x00000030
DATA 4 0x020E0284 0x00000030
DATA 4 0x020E04B0 0x00020000
DATA 4 0x020E0498 0x00000030
DATA 4 0x020E04A4 0x00000030
DATA 4 0x020E0244 0x00000030
DATA 4 0x020E0248 0x00000030
DATA 4 0x021B001C 0x00008000
DATA 4 0x021B0800 0xA1390003
DATA 4 0x021B080C 0x00010000
DATA 4 0x021B083C 0x4168016C
DATA 4 0x021B0840 0x00000000
DATA 4 0x021B0848 0x40405052
DATA 4 0x021B0850 0x40404E44
DATA 4 0x021B081C 0x33333333
DATA 4 0x021B0820 0x33333333
DATA 4 0x021B082C 0xf3333333
DATA 4 0x021B0830 0xf3333333
DATA 4 0x021B08C0 0x00921012
DATA 4 0x021B08B8 0x00000800
DATA 4 0x021B0004 0x0002002D
DATA 4 0x021B0008 0x1B333030
DATA 4 0x021B000C 0x676B52F3
DATA 4 0x021B0010 0xB64D0B63
DATA 4 0x021B0014 0x01FF00DB
DATA 4 0x021B0018 0x00201740
DATA 4 0x021B002C 0x000026D2
DATA 4 0x021B0030 0x006B1023
DATA 4 0x021B0040 0x0000004F
DATA 4 0x021B0000 0x84180000
DATA 4 0x021B001C 0x02008032
DATA 4 0x021B001C 0x00008033
DATA 4 0x021B001C 0x00048031
DATA 4 0x021B001C 0x15208030
DATA 4 0x021B001C 0x04008040
DATA 4 0x021B0020 0x00000800
DATA 4 0x021B0818 0x00000227
DATA 4 0x021B0004 0x0002556D
DATA 4 0x021B0404 0x00011006
DATA 4 0x021B001C 0x00000000
#endif

------------------------------------------------------------------------------------------------------

 

But when i am trying the flash the image, i am getting the following error .

ERROR : HID(R):LIBUSB_ERROR_TIMEOUT

Thanks...........

0 Kudos
Reply
1 Solution
6,063 Views
embedded_Dev
Contributor III

Yeah it is working now

View solution in original post

2 Replies
6,103 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Does it work now?

0 Kudos
Reply
6,064 Views
embedded_Dev
Contributor III

Yeah it is working now