ERROR: Fetcher failure: Unable to find revision 3c0874be4d3232d672b20f513451a39cfd7c585a in branch master even from upstream

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ERROR: Fetcher failure: Unable to find revision 3c0874be4d3232d672b20f513451a39cfd7c585a in branch master even from upstream

ソリューションへジャンプ
16,617件の閲覧回数
chandiniindavar
Contributor IV

Hi everyone

I am trying to build fsl-image-gui with yocto for imx7d board 

 i have successfully built the image and used it before without any problem ..

But this time i am getting below error : 

basavarajuc@ubuntu:/media/basavarajuc/ADD-New/fsl-release-bsp/YoctoIMX$ bitbake fsl-image-gui
WARNING: Host distribution "Ubuntu-16.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |##################################################################################| ETA: 00:00:00
Loaded 2826 entries from dependency cache.
Parsing recipes: 100% |################################################################################| Time: 00:00:01
Parsing of 2259 .bb files complete (2256 cached, 3 parsed). 2825 targets, 461 skipped, 5 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)
NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg

Build Configuration:
BB_VERSION = "1.28.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-16.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx7dsabresd"
DISTRO = "fsl-imx-fb"
DISTRO_VERSION = "4.1.15-1.2.0"
TUNE_FEATURES = "arm armv7a vfp neon callconvention-hard cortexa7"
TARGET_FPU = "vfp-neon"
meta
meta-yocto = "HEAD:dd0ba9ea4a11ab15348d4fe3574e4b28784db82f"
meta-oe
meta-multimedia = "HEAD:ad6133a2e95f4b83b6b3ea413598e2cd5fb3fd90"
meta-fsl-arm = "HEAD:35b8b9bd9863de208ab60e33b55f10ee43e2619b"
meta-fsl-arm-extra = "HEAD:e200df91b70da254461c59082ddd5db0a3c415a2"
meta-fsl-demos = "HEAD:2231e946e7a94d096394f2b2477e8184c9bbde7b"
meta-bsp
meta-sdk = "HEAD:dfbc90ee74624ce3be636c8bd2a47114fa2b71aa"
meta-browser = "HEAD:b6d46d69a261fe6bd7c1e9811dc2a9bbd0b79aeb"
meta-gnome
meta-networking
meta-python
meta-ruby
meta-filesystems
meta-xfce = "HEAD:ad6133a2e95f4b83b6b3ea413598e2cd5fb3fd90"
meta-qt5 = "HEAD:d5536e34ec985c82b621448ab4325e5cbba38560"

NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: Failed to fetch URL git://github.com/file/file.git, attempting MIRRORS if available
ERROR: Fetcher failure: Unable to find revision 3c0874be4d3232d672b20f513451a39cfd7c585a in branch master even from upstream
ERROR: Function failed: Fetcher failure for URL: 'git://github.com/file/file.git'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /media/basavarajuc/ADD-New/fsl-release-bsp/YoctoIMX/tmp/work/x86_64-linux/file-native/5.24-r0/temp/log.do_fetch.19333
ERROR: Task 669 (virtual:native:/media/basavarajuc/ADD-New/fsl-release-bsp/sources/poky/meta/recipes-devtools/file/file_5.24.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 306 tasks of which 305 didn't need to be rerun and 1 failed.
No currently running tasks (305 of 4157)

Summary: 1 task failed:
virtual:native:/media/basavarajuc/ADD-New/fsl-release-bsp/sources/poky/meta/recipes-devtools/file/file_5.24.bb, do_fetch
Summary: There were 2 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

Am i missing something ?

Anything has changed ?

I am referring attached guide to build image

ラベル(3)
0 件の賞賛
返信
1 解決策
14,093件の閲覧回数
raulatkinson
Contributor I

Try using this SRC_REV = "64503c1a161807380f4248c41d5d8d742893c819"

in the meta/recipes-devtools/file/file_5.24.bb  file...  Worked for me.  I had the exact same error as you.

from :

GitHub - file/file at FILE5_24 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
14,094件の閲覧回数
raulatkinson
Contributor I

Try using this SRC_REV = "64503c1a161807380f4248c41d5d8d742893c819"

in the meta/recipes-devtools/file/file_5.24.bb  file...  Worked for me.  I had the exact same error as you.

from :

GitHub - file/file at FILE5_24 

0 件の賞賛
返信
14,093件の閲覧回数
chandiniindavar
Contributor IV

Thanks for replay Raul..

It worked fine ... 

0 件の賞賛
返信