I'm having issues getting ENET1 to function on a custom board based off of the i.MX6UL dev kit. The interface works great in u-boot (can retrieve a DHCP address and respond to PING's). However, I've not had any luck getting it to work in the kernel.
here's my kernel version:
Linux version 4.1.20-01618-g0076509-dirty
Here are my DTS entries for the ethernet device:
pinctrl_enet1: enet1grp {
fsl,pins = <
MX6UL_PAD_ENET1_RX_EN__ENET1_RX_EN 0x1b0b0
MX6UL_PAD_ENET1_RX_ER__ENET1_RX_ER 0x13030
MX6UL_PAD_ENET1_RX_DATA0__ENET1_RDATA00 0x1b0b0
MX6UL_PAD_ENET1_RX_DATA1__ENET1_RDATA01 0x1b0b0
MX6UL_PAD_ENET1_TX_EN__ENET1_TX_EN 0x1b0b0
MX6UL_PAD_ENET1_TX_DATA0__ENET1_TDATA00 0x1b0b0
MX6UL_PAD_ENET1_TX_DATA1__ENET1_TDATA01 0x1b0b0
MX6UL_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x40000011
MX6UL_PAD_ENET2_RX_DATA0__ENET1_MDIO 0x0A429
MX6UL_PAD_ENET2_RX_DATA1__ENET1_MDC 0x1b088
>;
};
&fec1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_enet1>;
phy-mode = "rmii";
phy-handle = <ðphy0>;
phy-reset-gpios = <&gpio2 15 GPIO_ACTIVE_HIGH>;
phy-reset-duration = <500>;
status = "okay";
mdio {
#address-cells = <1>;
#size-cells = <0>;
ethphy0: ethernet-phy@1 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <1>;
};
};
};
When I try to configure the device, eth0, for static address these are the errors I receive:
sh-4.3# ifup eth0 -i etc/network/interfaces_static
run-parts: /etc/network/if-pre-up.d: No such file or directory
ifconfig: SIOCSIFFLAGS: No such device
ifconfig: SIOCSIFFLAGS: No such device
route: SIOCADDRT: Network is unreachable
sh-4.3# ip link set eth0 up
ip: SIOCSIFFLAGS: No such device
Any advice on using only ENET1 on the i.MX6UL?
Thanks in advance.