EMMC partition from kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EMMC partition from kernel

2,624件の閲覧回数
vinothkumars
Senior Contributor IV

Dear NXP,

 

I unable to create more partition from Linux,

by default,

 

root@imx8mnevk:~# ls -l /dev/mmcblk2*
brw-rw---- 1 root disk 179, 0 May 26 16:51 /dev/mmcblk2
brw-rw---- 1 root disk 179, 32 May 26 16:51 /dev/mmcblk2boot0
brw-rw---- 1 root disk 179, 64 May 26 16:51 /dev/mmcblk2boot1
brw-rw---- 1 root disk 179, 1 May 26 16:51 /dev/mmcblk2p1
brw-rw---- 1 root disk 179, 2 May 26 16:51 /dev/mmcblk2p2
crw------- 1 root root 237, 0 May 26 16:51 /dev/mmcblk2rpmb

 

I want to create mmcblk2p3 to mmcblk2p7. But, I unable to do it. will you please provide the proper steps or scripts to create EMMC partition from script or Linux commands

 

 

Regards,
Vinothkumar Sekar
ラベル(3)
タグ(5)
0 件の賞賛
返信
1 返信

2,617件の閲覧回数
b36401
NXP Employee
NXP Employee

You can use "fdisk" Linux command to manage EMMC partitions. Please refer to chapter 4.3.3 "Partitioning the SD/MMC card" of i.MX Linux User's Guide:
https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

0 件の賞賛
返信