EMC software guidelines for TFT RBG LCD with iMXRT1064

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EMC software guidelines for TFT RBG LCD with iMXRT1064

2,242 次查看
anujtanksali
Contributor II

Hi,

During EMC tests the 7" TFT RGB LCD is becoming white. What can be done in pin configuration or software to pass the EMC test? We already have implemented Spread spectrum using ref AN12879

with spread range of 24MHz and other all tests are passing except the 7" TFT RGB LCD

Am using iMXRT1064 and MCUXpresso IDE.

Thanks

Anuj

 

 

 

 

标签 (1)
0 项奖励
回复
5 回复数

2,219 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Normally when you have EMC problems it need to be solved by hardware modifications

 

Do you follow the recommendations on 

https://www.nxp.com/webapp/Download?colCode=MIMXRT105060HDUG

I hope this will help you

 

have a good day.

 

0 项奖励
回复

2,213 次查看
anujtanksali
Contributor II
Thanks for the reply
I understand the issues need to be resolved in hardware.
But are there any software guidelines to resolve the EMC issues?

I see some community posts mentioning to reduce the pin drive strength. Is this to be applied to all LCD, SDRAM or Backlight pins for only for clocks?

Thanks
Anuj
0 项奖励
回复

2,202 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Yes you can try that, also if this is possible you can test with different clock configurations, but maybe this is not a good option for your application

 

0 项奖励
回复

2,186 次查看
anujtanksali
Contributor II

Thanks for the reply.

As I see in MCUXpresso pin configuration the signal drive strength is represented in terms of R0/2, R0/4, R0/6 etc. Default setting is R0/6 

Can you please let me know the significance of this and It seems a lower setting should be set ie R0/4, R0/2, R0 to for reducing EMC issues?  Can you please confirm?

Thanks in advance

Anuj

 

0 项奖励
回复

2,134 次查看
anujtanksali
Contributor II

Hi,

Am Facing LCD ESD issues. The screen becomes white during ESD test when shocked with +-15kv. Can this be resolved in software using LCD Reset or by resetting some other LCD pins?.

If yes How do I reset the other LCD Pins as it seems the MCUXpresso does not allow to configure these pins except LCD DISP pin which is LCD reset.

Thanks

Anuj 

0 项奖励
回复