EIM problem on 4.1.15 kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EIM problem on 4.1.15 kernel

1,358 Views
lucaschettini
Contributor II

Hi,

we have a custom board based on iMX6 Q and D

We've few kernel modules, successfully compiled with both kernel 4.1.15 (on Ubuntu 16.04) and 3.14.54 (on Yocto Jethro).
These modules use EIM for comunicate with an FPGA connected to the EIM bus.

On 3.14.54 all works fine, but on 4.1.15 when I read data from EIM, I receive a static response data.

Correct data from 3.14.54:

FirmwareVersion: [b014] 45076
BuildYear: [2016] 8214
BuildMonthDay: [1027] 4135
BuildTime: [1130] 4400

Static data from 4.1.15:

FirmwareVersion: [2840] 10304

BuildYear: [2840] 10304
BuildMonthDay: [2840] 10304
BuildTime: [2840] 10304

If make a dump with a debugger on the corresponding virtual address, there are the same incorrect values at every EIM mapped address.

Are there changes from 3.14.54 to 4.1.15 EIM kernel implementation?
Have you an idea or suggestion?

TY
Luca

0 Kudos
Reply
1 Reply

1,239 Views
igorpadykov
NXP Employee
NXP Employee

Hi Luca

please try linux bsps descibed on nxp official i.mx page (use image

for sabre ai board which supports parallel nor)

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply