EIM RWSC Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EIM RWSC Configuration

1,653件の閲覧回数
674943148
Contributor II

Hi all,

I am learning the imx7D's WEIM module.

Is it possible to utilize different RWSC value on different CS? For example, i want to set the RWSC to 4 on CS0 and 3 on CS1. If possible, do i only need to configure the RWSC bits on EIM_CSnRCR1?

Best regards

ラベル(1)
2 返答(返信)

1,603件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wang

yes, it is possible to use different RWSC value on different CS, like to set the RWSC to 4 on CS0 and 3 on CS1.

Right, one needs to configure the RWSC bits on EIM_CSnRCR1.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,603件の閲覧回数
674943148
Contributor II

Hi igorpadykov,

Thank you! i'll check it out.

Best regards

0 件の賞賛
返信