EIM RWSC Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EIM RWSC Configuration

1,016 次查看
674943148
Contributor II

Hi all,

I am learning the imx7D's WEIM module.

Is it possible to utilize different RWSC value on different CS? For example, i want to set the RWSC to 4 on CS0 and 3 on CS1. If possible, do i only need to configure the RWSC bits on EIM_CSnRCR1?

Best regards

标签 (1)
2 回复数

966 次查看
igorpadykov
NXP Employee
NXP Employee

Hi wang

yes, it is possible to use different RWSC value on different CS, like to set the RWSC to 4 on CS0 and 3 on CS1.

Right, one needs to configure the RWSC bits on EIM_CSnRCR1.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

966 次查看
674943148
Contributor II

Hi igorpadykov,

Thank you! i'll check it out.

Best regards

0 项奖励
回复