EIM Performance impacted by Internal Bus Latency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EIM Performance impacted by Internal Bus Latency

1,483件の閲覧回数
richard_f
Contributor I

We have encountered the known issue regarding EIM bus cycle-to-cycle delay in our system recently.
We're using i.MX6DL with EIM interfacing to an FPGA, using asynch 32 bit multiplexed mode with DTACK.
Bus accesses are working fine, but we then discovered that there's excessive delay between successive CS assertions.

This is apparently a known limitation due to internal bus latency through PL301 cross bars and the AIPS peripheral bridge. (I've seen this explanation posted here by Yuri Muhin from NXP among others)
However, most of the posts by users who've experienced this issue were from well over a year or two ago. I have also seen a post from a user (PousseMousse - Jan 18, 2016) who claimed this issue was now resolved by the 1.3 Rev of the i.MX6S.

Can anyone at NXP or otherwise tell me whether this issue has been addressed/mitigated in any recent HW rev. of i.MX6DL, i.MX6S or even i.MX7D ?  

We are still in the early software development/evaluation phase and need to determine if this bus latency issue is a showstopper for our product application.  We had planned to evaluate the i.MX7D at some point in the near future as well.  So I am interested in knowing whether this issue exists to the same degree in that CPU as it does in i.MX6S/DL.

I have seen suggestions to use SDMA to mitigate the delay but we cannot make use of bursting, since successive writes to our FPGA are rarely if ever at contiguous longword addresses.

I would appreciate any updates on this issue as well as suggestions of tried and true ways to improve EIM performance.

thanks,
Richard F.

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 返信

1,355件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Richard

some details about i.MX6Q internal bus latencies may be obtained

creating service request.

How to create service request :
https://community.freescale.com/docs/DOC-329745

There are no known EIM latencies hardware improvements for 1.3 Rev of the i.MX6S,

also I am not aware of the same for i.MX7D.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信