寻求一款PSAM芯片,能够应用于Android 6.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

寻求一款PSAM芯片,能够应用于Android 6.0

887 Views
13102370205
Contributor I

NXP有没有一款SAM芯片可以支持在Android 6.0上应用,NXP可以给出相关应用资料。

0 Kudos
2 Replies

671 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Could you tell me which chip and board are you using?

Have a nice day

Rita

0 Kudos

670 Views
13102370205
Contributor I

你好!

我们的cpu 是mtk6737 我们本来想用pn7462完成NFC和管理SAM的,但是没有找到pn7462在Android系统的相关资料。现在我们想着用pn7150实现nfc的功能,SAM用其他芯片。你能给我们一个更好的方案吗?

期待你的答复

13102370205@163.com

发件人: b45499

发送时间: 2017-05-05 13:45

收件人: 小雨 李

主题: Re: - Re: 寻求一款PSAM芯片,能够应用于Android 6.0

NXP Community

Re: 寻求一款PSAM芯片,能够应用于Android 6.0

reply from Rita Wang in i.MX Community - View the full discussion

Hi,

Could you tell me which chip and board are you using?

Have a nice day

Rita

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in i.MX Community by email or at NXP Community

Following Re: 寻求一款PSAM芯片,能够应用于Android 6.0 in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 Kudos