EIM Internel Module Multiplexing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EIM Internel Module Multiplexing

1,587 Views
wanglee
Contributor III

I want to simply the  ADDRESS bus.  Please check the picture below.

EIM_Interface.JPG

Labels (1)
0 Kudos
Reply
1 Reply

1,495 Views
Yuri
NXP Employee
NXP Employee

Hello,

  It is not a problem (to leave floating high address lines) if these signals

are not used in Your device, connected to the EIM. Address range is defined

by CS. Please refer to Table 2-1 (System memory map) and section 22.4 (Chip
Select Memory Map)  of the Reference Manual.  CS must be used.

Note, address range will be restricted by low 16 bit.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply