EIM_EB3 boot configuration pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

EIM_EB3 boot configuration pin

跳至解决方案
34,353 次查看
rowangifford
Contributor II

I think there may be an error in the IMX6Q reference manual regarding one of the boot configuration pins.

From the IMX6Q reference manual page 269 pin EIM_EB3 is linked to boot configuration BOOT_CFG3[1]. Other pages also reference this (Table 4-2 page 327), Page 1974 IOMUXC_SW_MUX_CTL_PAD_EIM_EB3_B field descriptions.

However Table 8-3 on page 384 states EIM_EB3 is linked to BOOT_CFG4[7].

BOOT_CFG4[7] makes more sense as it is linked to the infinite loop test, whereas BOOT_CFG3[1] is reserved.

Which is correct?

Thanks,

Rowan

标签 (1)
0 项奖励
回复
1 解答
1,258 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rowan

yes, correct is Table 8-3 on page 384.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,259 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rowan

yes, correct is Table 8-3 on page 384.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------