EHCI failed to shut down host controller in uboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EHCI failed to shut down host controller in uboot

ソリューションへジャンプ
4,205件の閲覧回数
yashavanthashet
Contributor V

Hi all,

We are using imx_"3.14.38_6qp_ga yocto fido" bsp in our custom board. uboot version 2015.04.

In this after enabling usb in uboot when we boot the below error print is appearing.

""## Flattened Device Tree blob at 18000000

   Booting using the fdt blob at 0x18000000

EHCI failed to shut down host controller.

   Using Device Tree in place at 18000000, end 1801017d"

Could anybody tell me why this print is appearing and any solution for this issue.

Thanks in advance.

Regards,

Yashavantha

ラベル(3)
1 解決策
3,259件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yashavantha

seems this fixes below patch

[U-Boot] [PATCH 1/3] arm: mx6: cm-fx6: force host mode on usb controller

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
3,260件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yashavantha

seems this fixes below patch

[U-Boot] [PATCH 1/3] arm: mx6: cm-fx6: force host mode on usb controller

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,259件の閲覧回数
bhaskarkolkar
Contributor I

Hi yashavantha

are u able to fix the issue using the patch..

0 件の賞賛
返信