I'm using M4 core's ESCPI in i.max8mq and I want to start with the follow example code:
boards\evkmimx8mq\rtos_examples\freertos_ecspi\ecspi_loopback
boards\evkmimx8mq\driver_examples\ecspi\ecspi_loopback
Both of the 2 demos just run a single test on SPI then hung up CPU, just send 64 bytes and get the data back from internal loop. But the application scenario is to run SPI periodically. So I add a while(1) loop in the demo code, just like the following code segment. But the weird thing is the code stoped after several senonds. If I add the init function before transfer function the code can run all the time. Both the demo for RTOS and non-ROTS has the same issue. Does it nessary to initialise SPI before every signle transfer?
static void ecspi_task(void *pvParameters){
uint8_t i;
status_t status;
ecspi_rtos_handle_t master_rtos_handle;
ECSPI_MasterGetDefaultConfig(&masterConfig);
masterConfig.baudRate_Bps = ECSPI_TRANSFER_BAUDRATE;
masterConfig.enableLoopback = false;
for (i = 0; i < ECSPI_TRANSFER_SIZE; i++) {
masterTxData[i] = i;
}
while (1){
if (status != kStatus_Success) {
PRINTF("ECSPI meets error during initialization. \r\n");
vTaskSuspend(NULL);
}
masterXfer.txData = masterTxData;
masterXfer.rxData = masterRxData;
masterXfer.dataSize = ECSPI_TRANSFER_SIZE;
masterXfer.channel = ECSPI_MASTER_TRANSFER_CHANNEL; /*Start master transfer*/
status = ECSPI_RTOS_Transfer(&master_rtos_handle, &masterXfer);
if (status != kStatus_Success)
{
PRINTF("ECSPI transfer completed with error. \r\n\r\n");
vTaskSuspend(NULL);
} /* Compare Tx and Rx data. */
for (i = 0; i < ECSPI_TRANSFER_SIZE; i++)
{ if (masterTxData[i] != masterRxData[i])
{ break;
}
}
if (ECSPI_TRANSFER_SIZE == i)
{
PRINTF("\r\nFreeRTOS ECSPI loopback test pass!");
} else
{ PRINTF("\r\nFreeRTOS ECSPI loopback test fail!");
} }
vTaskSuspend(NULL);
}