ECSPI - MISO MOSI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ECSPI - MISO MOSI

1,889件の閲覧回数
neusch
Contributor II

Hello,

i woud like to connect two i.MX6 with SPI. (SCLK, MISO, MOSI, SS)

Reference Manual

[...]

21.4.2 Slave Mode

In this configuration, Chip Select (SS) becomes an input signal, and is used to control

data transfers through the Shift register, as well as to load/store the data FIFO.

[...]

-> Chip Select connected directly

But what i have to do with MISO/MOSI? Is crossing required?

[...]

ECSPI4_MISO (MISO) Master data in; slave data out EIM_D22
ECSPI4_MOSI (MOSI) Master data out; slave data in EIM_D28

[...]

i.MX6 Master - i.MX6 Slave

EIM_D22 (TX)  -  EIM_D28 (RX)

EIM_D28 (RX)  - EIM_D22 (TX)

or is no crossing required?

i.MX6 Master - i.MX6 Slave

EIM_D22 (TX)  -  EIM_D22 (RX)

EIM_D28 (RX)  - EIM_D28 (TX)

Thanks for any Help

ラベル(1)
1 返信

1,505件の閲覧回数
Yuri
NXP Employee
NXP Employee

SPI assumes the following connection :

Master MISO (MI) is connected to Slave MISO (SO)  

Master MOSI (MO) is connected to Slave MOSI (SI) 

So,

i.MX6 Master - i.MX6 Slave

EIM_D22 (TX)  -  EIM_D22 (RX)

EIM_D28 (RX)  - EIM_D28 (TX)