ECNR in IMX8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,069件の閲覧回数
M8
Contributor I

Hi,

1. Do all i.MX8 processors (i.MX8 mini including) support ECNR?

2. Also does i.MX8Mini support LPCM (Linear Pulse Code Modulated Audio), OPUS, AAC-LC (Advanced Audio Coding Low complexity), Mixer?

3. Is USB role switch supported in i.MX8 mini? What's the rated USB current for this processor?

Thanks

 

ラベル(1)
0 件の賞賛
返信
1 解決策
3,047件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

1. This solution is for 8 family, not 8M Mini family (MIMX8QM5AVUFFAB, MIMX8QM5CVUFFAB, MIMX8QM6AVUFFAB, MIMX8QM6CVUFFAB, MIMX8QP5AVUFFAB, MIMX8QP5CVUFFAB, MIMX8QP6AVUFFAB, MIMX8QP6CVUFFAB.)

But there is this solution tested on 8MM that features AEC.

2. They are tested under android (three of them).

3. It has two OTG interfaces compliant to.

josephlinares_0-1704768229620.pngjosephlinares_0-1704768229620.png

For a detailed current consumption description refer to datasheet.

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,024件の閲覧回数
M8
Contributor I

Hi,

Can you please share this doc? "14.8 USB Device Charger Detection Module (USBDCD) From reference manual"

Thanks

0 件の賞賛
返信
3,021件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

It exceeds the maximum size for attachments, please download it,

Regards,

0 件の賞賛
返信
3,035件の閲覧回数
M8
Contributor I

Hi Joseph Linares,

Thank you for the details.

A follow-up question on USB current rating.. 

I am interested to understand what modes can be supported in USB - SDP/CDP/etc? Per my understanding SDP requires 100mA and CDP is up to 1.5A. But based on the datasheet (table 63), the current output of the USB seems to be too low.. Should I be referring to any other data?

Thanks

 

 

0 件の賞賛
返信
3,031件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

They are not supported per se, you may want to refer to

14.8 USB Device Charger Detection Module (USBDCD)

From reference manual.

BC1.2 Spec is supported on 8M series (8M, 8MP, 8MN, etc).

Regards,

0 件の賞賛
返信
3,048件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

1. This solution is for 8 family, not 8M Mini family (MIMX8QM5AVUFFAB, MIMX8QM5CVUFFAB, MIMX8QM6AVUFFAB, MIMX8QM6CVUFFAB, MIMX8QP5AVUFFAB, MIMX8QP5CVUFFAB, MIMX8QP6AVUFFAB, MIMX8QP6CVUFFAB.)

But there is this solution tested on 8MM that features AEC.

2. They are tested under android (three of them).

3. It has two OTG interfaces compliant to.

josephlinares_0-1704768229620.pngjosephlinares_0-1704768229620.png

For a detailed current consumption description refer to datasheet.

Regards

0 件の賞賛
返信