Hi ,
I am working on imx53 customized board.I am able to boot Windows Embedded Compact 7 on ma platform.LCD driver is coming up properly.But my problem is I am not able to have two display's at the same time.I want to have both LCD and VGA working at the same and same contents.Please help me out in solving this.
Thanks in advance,
Seetharam
 
					
				
		
 justin_jiang
		
			justin_jiang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I uploaded the source code to the http://imxcommunity.org/group/wince/forum/topics/i-mx51-wince600-dual-display-set-di0-as-main-displa...
Dear Justin,
I checked "WINCE700\SUPPORT\APP\DisplaySet" and executed it on WinEC7 platform,
it will not call DisplayConfigureDual.
But I execute DisplaySet that you provide at this link, it will call DisplayConfigureDual.
Can you provide the source code of DisplaySet and mosquito_dual ?
Can secondary display play video ?
I am not familiar with DirectDraw, do you have any tutorial about DirectDraw to draw secondary display.
Dear Seetharam,
Can you share how to enable dual display in WinEC7 with same content or different content ?
Thx ~
 Jiang Justin said:
for current WinCE dual display solution, you need use displaySet app in "WINCE600\SUPPORT\APP\DisplaySet" to enable the secondary display. It will call DisplayConfigureDual().
Please check the attach RM for the details about the dual display.
 
					
				
		
 justin_jiang
		
			justin_jiang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Sorry, I have just enabled a dual display on ce6 with mx51 platfrom. but since the code architecture and ipu is almost same, so i think you can have a refer to it.
Thanks Justin for your reply. BSP_ENABLE_SECONDARY_PRIMARY_SURFACE variable is set but what exactly happening is in displaysetmode() function of display.cpp first it is checking for DI0 panel and if its connected then it will not check for DI1.VGA is connected to DI1 and DisplayConfigureDual() function is not at all getting called.Please help me in solving this.
Thanks and Regards,
Seetharam
 
					
				
		
 justin_jiang
		
			justin_jiang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Please check the "DisplayConfigureDual()" in display.cpp and make sure to set
#define BSP_ENABLE_SECONDARY_PRIMARY_SURFACE TRUE.