Dual Display on IMX6Q in Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual Display on IMX6Q in Android

Jump to solution
13,795 Views
johnturnur
Contributor III

Hi,

I have IMX6Q SABRE SDB bouard.

I am using pre-build android image to get Dual display working on IMX6Q. (android 13.4.1).

I want to get dual display output with HDMI and LCD display.

Following bootargs i have used. But I am not able to get any success. I got output in ant one display not on both.

setenv bootargs console=ttymxc0,115200 video=mxcfb0:dev=lcd,800x480M@60,if=RGB24,bpp=32 video=mxcfb1:dev=hdmi,1920x1080M@60 video=mxcfb2=off fbmem=28M

Any sugettions for my issue.

Thanks,

John

Labels (5)
Tags (3)
1 Solution
4,770 Views
lily_zhang
NXP Employee
NXP Employee

Regarding "HDMI + LCD",  Please try "setenv bootargs console=ttymxc0,115200 video=mxcfb0: lcd,CLAA-WVGA@60,if=RGB565,bpp=32 video=mxcfb1: dev=hdmi,1920x1080M@60 video=mxcfb2:off fbmem=5M,28M".

View solution in original post

0 Kudos
Reply
16 Replies
4,770 Views
增超段
Contributor I

Hi! How to set hdmi display on or off depending on the situation dynamically?

0 Kudos
Reply
4,770 Views
conteczxy
Contributor III
0 Kudos
Reply
4,770 Views
daiane_angolini
NXP Employee
NXP Employee

Following the Advanced User Guide I was able to share my UI on HDMI display:

(I´m using LVDS, please try using WVGA and let me know if works the same way)

1 -

setenv bootargs console=ttymxc0,115200 init=/init rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666

fb0base=0x27b00000

video=mxcfb1:dev=hdmi,1920x1080M@60 fbmem=10M,28M vmalloc=400M

2- Start the Advanced display setting by clicking HDMI notification in the Status bar.

3- Enable the HDMI display by clicking the "Enable Display", which will make the Android UI show in both LVDS and

HDMI display.

Please, let me know the result

0 Kudos
Reply
4,770 Views
soujanyak
Contributor I

Hello,

I downloaded the source code for Sabre-SD board, jelly bean android OS.

I am able to build the code and boot it also.

But when i am trying to do dual boot with LVDS as primary display and HDMI as secondary display i am unable to get anything on either of the displays, the following are the boot-args being used to enable dual display :

setenv bootargs console=ttymxc0,115200 init=/init rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb1:dev=hdmi,1920x1080M@60 fbmem=10M,28M vmalloc=400M

Please let me know what else have to be done.

0 Kudos
Reply
4,770 Views
lily_zhang
NXP Employee
NXP Employee

In JB4.2.2 Quick Start, you can get the command for Dual display:

3.4.3 Booting with Dual Displays: LVDS and HDMI Displays

In the U-Boot prompt, set the U-Boot environment variables as shown below:

U-Boot > setenv bootcmd booti mmc3

U-Boot > setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 vmalloc=400M

init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:dev=hdmi,1920x1080M@60,bpp=32

video=mxcfb2:off fbmem=10M androidboot.hardware=freescale

U-Boot > saveenv

If you find it can not work, please check your boot log and see whether the display is detected


0 Kudos
Reply
4,770 Views
erictheis
Contributor I

I've gotten this to work. But I want to not mirror the same contents to both displays.

I want to have two separate and different contents on each display. How?

- Eric

0 Kudos
Reply
4,770 Views
daiane_angolini
NXP Employee
NXP Employee

I will not be able to test it myself until next Wednesday  - I'm sorry -

Did you tried the command lines separated? (once for LVDS, once for HDMI?)

Could you, please, check the User Guide in order to see the command line you need to include (it's something related with setprop.dualXXX) in order to get dual display enabled on Android?

0 Kudos
Reply
4,770 Views
PrabhuSundarara
NXP Employee
NXP Employee

Can you please try with

video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 ldb=dul0 to boot up on LVDS and then you change. Please keep posted whether it fixes the problem.

4,770 Views
johnturnur
Contributor III

I want to get dual display one with HDMI and LCD.

0 Kudos
Reply
4,771 Views
lily_zhang
NXP Employee
NXP Employee

Regarding "HDMI + LCD",  Please try "setenv bootargs console=ttymxc0,115200 video=mxcfb0: lcd,CLAA-WVGA@60,if=RGB565,bpp=32 video=mxcfb1: dev=hdmi,1920x1080M@60 video=mxcfb2:off fbmem=5M,28M".

0 Kudos
Reply
4,770 Views
_benjamindubb
Contributor II

Is it even possible to have two displays show different output in Android? I don't think Google supports that, but I'd love to be proven wrong.

I'd actually want one framebuffer to span across two LVDS panels. Can it be done with i.MX6?

Thanks,

-Ben

0 Kudos
Reply
4,770 Views
lily_zhang
NXP Employee
NXP Employee

JellyBean 4.2 supports multiple display. Different contents can be supported.

0 Kudos
Reply
4,770 Views
johnturnur
Contributor III

where can i found JellyBean ?

0 Kudos
Reply
4,770 Views
lily_zhang
NXP Employee
NXP Employee

You can contact sales or marketing to get Jelly Bean information.

4,770 Views
lily_zhang
NXP Employee
NXP Employee


Try this for LCD "setenv bootargs console=ttymxc0,115200 video=mxcfb0: lcd,CLAA-WVGA@60,if=RGB565,bpp=32 video=mxcfb1: dev=hdmi,1920x1080M@60 video=mxcfb2: off fbmem=5M,28M".

If it doesn't work, please send out the logs.

4,770 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Ticket was  already create for this  issue, SR 1-1006680555.

It was assigned and  follow up will be provided in the  SR.

0 Kudos
Reply