Driving LEDs with iMXRT1064

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Driving LEDs with iMXRT1064

ソリューションへジャンプ
1,457件の閲覧回数
etronic_arg
Contributor III

Hello,

I want to connect 8 LEDs (4mA each, 32mA total) directly to GPIO pins.
Is it possible?
or it should be necessary to add a driver?

I couldn't find the total maximum current in the datasheet. The only information is the maximum current of a pin, +/-4mA depending on the ipp_dse value.

Thanks

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,446件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to table 22 in the data sheet of i.mxrt1060, the current of each I/O cell in push/pull output mode is +/-1mA(sink/source current), so you have to connect a transistor or mosfet to drive led if it requires 4mA current.

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1670484942313.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,447件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to table 22 in the data sheet of i.mxrt1060, the current of each I/O cell in push/pull output mode is +/-1mA(sink/source current), so you have to connect a transistor or mosfet to drive led if it requires 4mA current.

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1670484942313.png

 

0 件の賞賛
返信