Driver for Parallel Image Sensor AR0134

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Driver for Parallel Image Sensor AR0134

3,584件の閲覧回数
rajabalaji
Contributor II

Hi,

Do freescale provide driver for AR0134 ? or any other parallel image sensor? Has anyone else developed it? If I have to start editing for this specific sensor, suggest me a driver with which I can use as a base ?

PS: I am looking for a Image sensor with Global shutter for Machine Vision application. Any other sensor that fits would also be fine. 

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,675件の閲覧回数
茂实丁
Contributor II

you can modify the ov5640.c in subdev directory. Driver's structure is similar.

0 件の賞賛
返信

2,675件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raja

no this driver is not provided. Provided drivers for ov5640,5642

one is mipi, other parallel. Description of linux drivers one can find in

attached Linux Manual Chapter 6 Image Processing Unit (IPU) Drivers.

Bare metal examples can be found in

"MX6_PLATFORM_SDK "

i.MX6 Platform SDK 1.1 Release

Example of connection in i.MX6_SABRE_SDP_DESIGNFILES

SABRE for Smart Devices Reference Design|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信