Driver for Linux for Freescale i.MX53 Sabre tablet reference design platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Driver for Linux for Freescale i.MX53 Sabre tablet reference design platform

1,268 Views
allenwong
Contributor II

Hello,

My customer has purchased this Freescale i.MX53 Sabre Tablet.

Previously, they are unable to find any update on the development platform which include various source codes and device drivers which is required to build the system before they are able to talk to various flavors of Android which lie on the top of embedded LINUX operating system.

Just wondering if FSL managed to release any new software platform?

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX53SABRETAB&fpsp=1&tab=Design_Too...

Seems like there is not much update since 2013.

Thanks for your time for replying my questions.

Labels (2)
0 Kudos
Reply
1 Reply

1,149 Views
igorpadykov
NXP Employee
NXP Employee

Hi Allen

latest official BSP releases can be found on link below

SABRE Platform for Tablets Reference Design|Freescale

Also one can use community software, links below, these are

more frequently updated.

FSL Community BSP Release Notes 1.7 documentation

http://freescale.github.io/doc/release-notes/1.7/index.html

Index of /releases/yocto/yocto-1.6/machines/imx53qsb

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply