Driver Monitoring System Demo - i.mx93evk

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Driver Monitoring System Demo - i.mx93evk

3,312 次查看
jcase
Contributor II

Hello,

I have an imx93evk and have been exploring the latest provided Langdale image. It seems there are two driver monitoring system demos, one within the demo experience and another under eiq examples folder. 

Is the source code available on NXP github for both driver monitoring systems? If so, can you please help point me to it?

Thank you.

标签 (1)
0 项奖励
回复
2 回复数

3,254 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

On the board, please go to the next path to check the DMS source code:

$ cd /home/root/.nxp-demo-experience/scripts/machine_learning/dms

Jorge7u7_0-1695916776093.png

Best regards.

0 项奖励
回复

3,224 次查看
jcase
Contributor II

Hello,

Thanks for the reply. Yes, I have been referencing the code contained within the latest image that was released from NXP for the driver monitoring system. However, there may be another version that was not packaged in the image or distributed via github?

More specifically, I was wondering if the source code for the demo below is available?

jcase_0-1696535576194.png

Thank you.

-Jacob

 

0 项奖励
回复