Download for Android L5.0.0_1.0.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Download for Android L5.0.0_1.0.0

ソリューションへジャンプ
2,819件の閲覧回数
EricNelson
Senior Contributor II

Hi all,

I see links for the Lollipop release on this page, but the download links don't

appear to be functioning.

     Android OS for i.MX Applications Processors|Freescale

Is this a known issue?

ラベル(2)
0 件の賞賛
返信
1 解決策
2,596件の閲覧回数
cyborgnegotiato
Senior Contributor II

Hi,

which one?

IMX6-L500-100-ANDROID-SOURCE-BSP works for me...

Regards,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,597件の閲覧回数
cyborgnegotiato
Senior Contributor II

Hi,

which one?

IMX6-L500-100-ANDROID-SOURCE-BSP works for me...

Regards,

Jozef

0 件の賞賛
返信
2,596件の閲覧回数
EricNelson
Senior Contributor II

Hi Jozef,

That's the one, and it's now working for me as well.

I and a colleague tried several times since yesterday and were stuck waiting for the download.

0 件の賞賛
返信