Download for Android L5.0.0_1.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Download for Android L5.0.0_1.0.0

Jump to solution
1,455 Views
EricNelson
Senior Contributor II

Hi all,

I see links for the Lollipop release on this page, but the download links don't

appear to be functioning.

     Android OS for i.MX Applications Processors|Freescale

Is this a known issue?

Labels (2)
0 Kudos
Reply
1 Solution
1,232 Views
cyborgnegotiato
Senior Contributor II

Hi,

which one?

IMX6-L500-100-ANDROID-SOURCE-BSP works for me...

Regards,

Jozef

View solution in original post

0 Kudos
Reply
2 Replies
1,233 Views
cyborgnegotiato
Senior Contributor II

Hi,

which one?

IMX6-L500-100-ANDROID-SOURCE-BSP works for me...

Regards,

Jozef

0 Kudos
Reply
1,232 Views
EricNelson
Senior Contributor II

Hi Jozef,

That's the one, and it's now working for me as well.

I and a colleague tried several times since yesterday and were stuck waiting for the download.

0 Kudos
Reply