Hi,
Regarding i.MX Plus EVK(evk_8mp) Ethernet ENET2(J8)
The attached file (patch file) is for #2_Ethernet Port on IMX8MP EVK. for Android 11.0.0_2.4.0, ethernet ENET2(ENET2:J8)..
This patch file is working well based on Android 11.0.0_2.4.0.
Then, Its patch file is not working based on the android 12.0.0_1.0.0 for #2 Ether port please ** i.MX 8MPlus EVK(evk_8mp) Ethernet ENET2(J8)
What is the problem?
** Original Android BSP for IMX8MP is not working for ENET2(ENET2:J8) on the IMX8MP EVK
已解决! 转到解答。
Hi,
thank a lot for the answer.
But is the package compatible with Android 12?
When I apply the patch "0001-android-vendor-fsl_imx_demo-dual-ethernet-demo.patch",
I have the Android.bp.rej file and some files that the patch should delete are not present.
Best Regards
Domenico Acri