Don’t work Ethernet Port (ENET2:J8) of IMX8MPlus EVK Based on android 12.0.0_1.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Don’t work Ethernet Port (ENET2:J8) of IMX8MPlus EVK Based on android 12.0.0_1.0.0

Jump to solution
2,879 Views
kiwonlee1
Contributor II

Hi,

Regarding i.MX Plus EVK(evk_8mp) Ethernet ENET2(J8)

The attached file (patch file) is for #2_Ethernet Port on IMX8MP EVK. for Android 11.0.0_2.4.0, ethernet ENET2(ENET2:J8)..

This patch file is working well based on Android 11.0.0_2.4.0.

Then, Its patch file is not working based on the android 12.0.0_1.0.0 for #2 Ether port please ** i.MX 8MPlus EVK(evk_8mp) Ethernet ENET2(J8)

 

What is the problem?

 

** Original Android BSP for IMX8MP is not working for ENET2(ENET2:J8) on the IMX8MP EVK

0 Kudos
Reply
1 Solution
2,869 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I give update in the case you create, please check it, so close it here.

Wish you have a nice day

View solution in original post

0 Kudos
Reply
13 Replies
2,870 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I give update in the case you create, please check it, so close it here.

Wish you have a nice day

0 Kudos
Reply
2,398 Views
Miles_x
Contributor I

Hi,   I also use android 12.0.0_1.0.0 for dual ethernet port, please send me the update file, thanks!

0 Kudos
Reply
1,978 Views
domenicoacri
Contributor III

Hi, I also use android 12.0.0_1.0.0 for dual ethernet port, please send me the update file, thanks!

0 Kudos
Reply
1,952 Views
kiwonlee1
Contributor II
0 Kudos
Reply
1,582 Views
domenicoacri
Contributor III

Hi,

Thank you so much.


Could you reshare the file as I can no longer download it?

 

BR

Domenico Acri

0 Kudos
Reply
1,568 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I email to you just now, please check it.

0 Kudos
Reply
1,228 Views
JungWonLee
Contributor I

Hi, I use android 12.0.0_2.0.0 for dual ethernet port, please send me the update file, thanks!

0 Kudos
Reply
1,219 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

@JungWonLee I already email to you, please have a check.

Wish you have a nice day

1,212 Views
JungWonLee
Contributor I
Thank you so much
0 Kudos
Reply
1,536 Views
domenicoacri
Contributor III

Hi Rita_Wang,

do you happen to have an EthernetDual package for Android 12?

Or even the apk?

 

BR

Domenico Acri

0 Kudos
Reply
1,548 Views
domenicoacri
Contributor III

Hi,

thank you very much.

You could also send me the patches:

0001-android-vendor-fsl_imx_demo-dual-ethernet-demo.patch

.....

to include the project?

 

BR

Domenico Acri

0 Kudos
Reply
1,942 Views
domenicoacri
Contributor III

Hi,

thank a lot for the answer.

But is the package compatible with Android 12?

When I apply the patch "0001-android-vendor-fsl_imx_demo-dual-ethernet-demo.patch",

I have the Android.bp.rej file and some files that the patch should delete are not present.

 

Best Regards

Domenico Acri

0 Kudos
Reply
2,382 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

@Miles_x I already email to you, please have a check.

Wish you have a nice day

Best Regards

Rita

0 Kudos
Reply