Does the IVT( Interrupt vector table) part of the FCB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does the IVT( Interrupt vector table) part of the FCB

807 次查看
adityanagal
Contributor III

Hi ,

As per the IMX reference Manual , section 8.5.5.2 ,

"As part of the NAND media initialization, the ROM driver uses safe NAND timings to

search for a Firmware Configuration Block (FCB) that contains the optimum NAND

timings, page address of Discovered Bad Block Table (DBBT) Search Area and start

page address of primary and secondary firmware "

So as per my understanding , Interrupt Vector table should be part of the FCB data structure . Please let me know if it is not so.

Regards,

Aditya Nagal

0 项奖励
回复
1 回复

715 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

no, Interrupt Vector table is not part of the FCB data structure.

Details can be found in Boot Chapter of processor Reference Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复