Does mfgtool support SPL uboot?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does mfgtool support SPL uboot?

2,257 次查看
robinkwek
Contributor I

Hi,

We’d like to use SPL uboot in coming project to handle initialization of different DDR RAM models (due to EOL).

However, if mfgtool doesn’t support SPL uboot, it’s quite awkward to support 2 mode of uboot in one project and defeat the purpose of SPL uboot.

I’d like to know if NXP would support SPL uboot in mfgtools or NXP has any other method to solve this issue.

Thanks.

0 项奖励
回复
3 回复数

1,942 次查看
robinkwek
Contributor I

Hi Igor,

May I know whether mfgtool is an open source?

Any way we can get the source code?

Thanks.

Regards,

Robin

0 项奖励
回复

1,942 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Robin

please look at

i.MX6Q|i.MX 6Quad Processors|Quad Core|NXP

Programmers (Flash, etc.) (13)

Source Code for the i.MX manufacturing tool used for downloading OS images

to the i.MX 6 Processors (REV 2.3.2)

~igor

0 项奖励
回复

1,942 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Robin

you are right, mfg tool does not support spl uboot, I am not

aware of plans for its integration. In general one can apply to

to NXP Professional Services for that:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

[email protected]

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复