Does imx6 android support two camera run at the same time

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does imx6 android support two camera run at the same time

3,341 次查看
lipeng1
Contributor I

dear all

I use the saberd imx6q,i want two camera run at the same time ,now the driver and hardware can support two camera run at same time ,but i don not  know if android can show two camera at the same

标签 (2)
0 项奖励
回复
8 回复数

2,631 次查看
igorpadykov
NXP Employee
NXP Employee

Hi lipeng

please check below

android-imx6-kitkat/0237-ENGR00174526-Add-dual-camera-feature-into-mx6-ICS.patch at master · rabeeh/...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,631 次查看
lipeng1
Contributor I

dear igorpadykov

thanks for your reply

the patch you give me used for libcamera ,but the sabresd_6dq used the  libcamera2(IMX_CAMERA_HAL_V2),

Do you have patch for libcamera2 ? 

thanks

0 项奖励
回复

2,631 次查看
lipeng1
Contributor I

and the patch you give me only used for two camera swicth,not for  two camera run at the same time 

0 项奖励
回复

2,631 次查看
igorpadykov
NXP Employee
NXP Employee

Hi lipeng

you can use usb camera as well.

~igor

0 项奖励
回复

2,631 次查看
lipeng1
Contributor I

do you mean use two usb camera same time?

0 项奖励
回复

2,631 次查看
igorpadykov
NXP Employee
NXP Employee

any configuration is possible

0 项奖励
回复

2,631 次查看
lipeng1
Contributor I

now android4.2.2 can support two camera show sametime ?(imx6 sabresd_6dq

0 项奖励
回复

2,631 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复