Does i.MX8MQ have OpenVX support available?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX8MQ have OpenVX support available?

2,240 Views
chandresh_tank
Contributor II

I am trying to port an OpenCV based application from iOS to i.MX8MQ based platform in which i have connected IMX334 based sony camera to its MIPI CSI bus. 

I have created the yocto build and varified on the board, In the /opt/imx-gpu-sdk/ directory, It has OpenCL and OpenVG support with their sample application?

Can we add OpenVX support in imx8MQ and if so, and How can i enabled OpenVX support and its example applications in yocto build? openvx #imx8mq

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

2,133 Views
joanxie
NXP TechSupport
NXP TechSupport

currently imx8qm and imx8mp support openVX, refer to the imx8MQ reference manual, imx8MQ doesn't support openVX, for more detailed information, you can refer to the document as below

https://community.nxp.com/docs/DOC-345644 

1,452 Views
EdSutter
Senior Contributor II

This needs some clarification (for me anyway)...

The document you point to (https://community.nxp.com/docs/DOC-345644) implies that the iMX8MP supports OpenVX; however looking at the features table for the different varieties of iMX8 here https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces... the iMX8MP doesn't have the OpenVX box checked...

@joanxie , would you be able to confirm whether or not the iMX8MP supports OpenVX?

Thanks,

0 Kudos
Reply