In i.MX8M reference manual revision 1.
1.6 says support boot from NAND, SDIO/MMC/SDXC, eMMC, SPI, USB, QSPI and Ethernet.
6.1 says support boot from SD/MMC and NAND flash.
Which one is right?
Solved! Go to Solution.
Hello m.c.
Both are rigth the i.MX8M can boot from NAND, SDIO/MMC/SDXC, eMMC, SPI, USB, QSPI and Ethernet, but the boot ROM suport NAND and SD/MMC, The boot ROM uses the state of the BOOT_MODE and eFUSEs to determine the boot
device. For development purposes, the eFUSEs used to determine the boot device may be overridden using the GPIO pin inputs.
Regards
Hello m.c.
Both are rigth the i.MX8M can boot from NAND, SDIO/MMC/SDXC, eMMC, SPI, USB, QSPI and Ethernet, but the boot ROM suport NAND and SD/MMC, The boot ROM uses the state of the BOOT_MODE and eFUSEs to determine the boot
device. For development purposes, the eFUSEs used to determine the boot device may be overridden using the GPIO pin inputs.
Regards
Hi Bio_TICFSL,
i don't get it.
This thread (https://community.nxp.com/thread/473293) is saying that there is no boot options from QSPI.
So how do i implement booting from QSPI after your statement.
Thanks in advance!
Best regards,
Juergen