Does i.MX8M support boot from QSPI?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does i.MX8M support boot from QSPI?

ソリューションへジャンプ
1,558件の閲覧回数
m_c
Senior Contributor I

In i.MX8M reference manual revision 1.

1.6 says support boot from NAND, SDIO/MMC/SDXC, eMMC, SPI, USB, QSPI and Ethernet.

pastedImage_2.png

6.1 says support boot from SD/MMC and NAND flash.

pastedImage_1.png

Which one is right?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,264件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello m.c.

Both are rigth the i.MX8M can boot from NAND, SDIO/MMC/SDXC, eMMC, SPI, USB, QSPI and Ethernet, but the boot ROM suport NAND and SD/MMC, The boot ROM uses the state of the BOOT_MODE and eFUSEs to determine the boot
device. For development purposes, the eFUSEs used to determine the boot device may be overridden using the GPIO pin inputs.

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,265件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello m.c.

Both are rigth the i.MX8M can boot from NAND, SDIO/MMC/SDXC, eMMC, SPI, USB, QSPI and Ethernet, but the boot ROM suport NAND and SD/MMC, The boot ROM uses the state of the BOOT_MODE and eFUSEs to determine the boot
device. For development purposes, the eFUSEs used to determine the boot device may be overridden using the GPIO pin inputs.

Regards

0 件の賞賛
返信
1,264件の閲覧回数
juergene
Contributor III

Hi Bio_TICFSL,

i don't get it. 

This thread (https://community.nxp.com/thread/473293) is saying that there is no boot options from QSPI.

So how do i implement booting from QSPI after your statement.

Thanks in advance!

Best regards,

Juergen

#i.mx8m

0 件の賞賛
返信