Does i.MX6SL have touch screen interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6SL have touch screen interface?

Jump to solution
1,850 Views
JHY
Contributor IV

Seeing a block diagram in IMX6SLRM 1.5.1, it looks like i.MXSL has Touch Panel Control.

Is there interfaces for touch panel  in IMX6SL?

Otherwise if I build HW using ADC or GPIO, can I be provided some SW drivers?

Regards.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,707 Views
Yuri
NXP Employee
NXP Employee

The i.MX6 SL does not have embedded touch / ADC interface, sorry.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,708 Views
Yuri
NXP Employee
NXP Employee

The i.MX6 SL does not have embedded touch / ADC interface, sorry.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply