Does anyone have patch for rpmsg wakeup source for kernel L4.1.15

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does anyone have patch for rpmsg wakeup source for kernel L4.1.15

ソリューションへジャンプ
3,345件の閲覧回数
rakesh_patel
Senior Contributor I

Hi,

As per below document,

iMX8QXP: Use RPMSG to wake up M4 and A35 

patch : L4.14.78_rpmsg_wakeup.patch is for only L4.14.78.

Is there any patch for L4.14.15 as I see there are many changes in rpmsg kernel changes and it looks like not easy to port L4.14.78 patch to L4.1.15?

 

ラベル(1)
0 件の賞賛
返信
1 解決策
3,134件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rakesh

I am afraid such patch is not available for L4.1.15, also it is very old kernel

version no more supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,135件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rakesh

I am afraid such patch is not available for L4.1.15, also it is very old kernel

version no more supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,134件の閲覧回数
rakesh_patel
Senior Contributor I

igorpadykov‌:

In kernel 4.1.15, rpmsg wakeup is default enabled. So it required no patch.

Thanks for your support.

0 件の賞賛
返信
3,134件の閲覧回数
vinothkumars
Senior Contributor IV

Hi Rakesh Patel

Will you please tell me how you done RPMSG wakeup.

Regards,

Vinoth S,

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
3,134件の閲覧回数
rakesh_patel
Senior Contributor I

RPMSG is default wakeup source. You don't require any changes.vinothkumars

0 件の賞賛
返信
3,134件の閲覧回数
vinothkumars
Senior Contributor IV

Hi [email protected]‌

I am using latest kernel L4.14.98

Will you please give the patch for Rpmsg or will you please tell me how you done Rpmsg wakeup

Thanks,

Vinoth S,

Regards,
Vinothkumar Sekar
0 件の賞賛
返信