Does anyone have patch for rpmsg wakeup source for kernel L4.1.15

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does anyone have patch for rpmsg wakeup source for kernel L4.1.15

Jump to solution
3,348 Views
rakesh_patel
Senior Contributor I

Hi,

As per below document,

iMX8QXP: Use RPMSG to wake up M4 and A35 

patch : L4.14.78_rpmsg_wakeup.patch is for only L4.14.78.

Is there any patch for L4.14.15 as I see there are many changes in rpmsg kernel changes and it looks like not easy to port L4.14.78 patch to L4.1.15?

 

Labels (1)
0 Kudos
Reply
1 Solution
3,137 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rakesh

I am afraid such patch is not available for L4.1.15, also it is very old kernel

version no more supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
3,138 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rakesh

I am afraid such patch is not available for L4.1.15, also it is very old kernel

version no more supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,137 Views
rakesh_patel
Senior Contributor I

igorpadykov‌:

In kernel 4.1.15, rpmsg wakeup is default enabled. So it required no patch.

Thanks for your support.

0 Kudos
Reply
3,137 Views
vinothkumars
Senior Contributor IV

Hi Rakesh Patel

Will you please tell me how you done RPMSG wakeup.

Regards,

Vinoth S,

Regards,
Vinothkumar Sekar
0 Kudos
Reply
3,137 Views
rakesh_patel
Senior Contributor I

RPMSG is default wakeup source. You don't require any changes.vinothkumars

0 Kudos
Reply
3,137 Views
vinothkumars
Senior Contributor IV

Hi [email protected]‌

I am using latest kernel L4.14.98

Will you please give the patch for Rpmsg or will you please tell me how you done Rpmsg wakeup

Thanks,

Vinoth S,

Regards,
Vinothkumar Sekar
0 Kudos
Reply