Does WDT keep running after kernel crash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does WDT keep running after kernel crash?

1,600 Views
viniciusmaciel
Contributor II

Hi,

I want to know if the Watchdog timer continue to run even after the linux kernel crash?

In my current system, Linux 4.9.11 on wandboard, after the linux kernel crashes nothing happen and  I have to reboot manually, which will not be possible when my system goes to field.

Labels (3)
Tags (2)
0 Kudos
Reply
1 Reply

1,459 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vinicius

in general it should work except cases, when accidentally

wdt clock sources were disabled, described in sect.70.3 Clocks

Chapter 70 Watchdog Timer (WDOG) i.MX6SDL Reference
Manual or changed bits WDZST, WDBG, register WDOGx_WCR.
http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply