Does MX6ULL support Serial/SPI NAND?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MX6ULL support Serial/SPI NAND?

1,543 Views
ScottKerstein
Contributor III

Hello,

Serial/SPI NAND Flash offers advantages for lower memory densities, but it's not clear in the datasheet if it supports Serial/SPI NAND?  eMMC is supported and desirable because of the error management built inside.  Since Serial/SPI NAND can be used reliably in systems that provide bad-block management and error-correction algorithms, it looks like I have to this management in the i.MX6ULL.

Does the MX6ULL support Serial/SPI NAND with 8-bit ECC?

Thanks in advance,

Scott

Labels (2)
0 Kudos
Reply
1 Reply

1,301 Views
igorpadykov
NXP Employee
NXP Employee

Hi Scott

supported serial memory devices, such as EEPROM and serial flash, using the SPI,

Serial/SPI NAND not supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply