Does MFGtool need to be updated to program the uboot over Raw Nand Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MFGtool need to be updated to program the uboot over Raw Nand Flash

818 Views
adityanagal
Contributor III

Hi , 

I am working over the IMX6 solo based Target board on which IMX6 solo is interfaced with Raw Nand Flash over GPMI interface. Raw Nand Flash is used as a booting option. My questions are :

1. Can we program raw Nand Flash using MFG tool . 

2. Do we need to customize/update the MFGtool to program the Nand Flash. 

Please Suggest.

Regards,

Aditya Nagal

0 Kudos
Reply
1 Reply

732 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Here you can use the mfgtool to download images to nand, but you need to do some modify in the mfgtool. Could you tell me which version BSP are you using?
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply