Does MCIMX6SX-SDB have emmc interface?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does MCIMX6SX-SDB have emmc interface?

跳至解决方案
3,245 次查看
JHY
Contributor IV

SPF-27962.pdf describes that MCIMX6SX-SDB has only foot print for eMMC interface.

Is it possble to test eMMC using MCIMX6SX-SDB?

e.jpg

标签 (1)
标记 (1)
1 解答
3,020 次查看
igorpadykov
NXP Employee
NXP Employee

Hi JHY

eMMC can be used after soldering on this foot print, for tests

one can follow sect.4.4.1.2 Using eMMC attached Linux Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
3,021 次查看
igorpadykov
NXP Employee
NXP Employee

Hi JHY

eMMC can be used after soldering on this foot print, for tests

one can follow sect.4.4.1.2 Using eMMC attached Linux Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------